Technical FAQs

Ask a Question

Which side of an oil-filled padmount medium voltage transformer is customaryily the high voltage side?

The left side, as viewed from the front, is normally the high voltage side.


CTA-ID : 2003813
Was this helpful?
What can we do to improve the information ?