Technical FAQs

Ask a Question

Do the busway End Closures install on the bolt end or slot end of the busway? <br />

The End Closure can be mounted on either the bolt or slot end of the busway. Refer to installation instructions included with the End Closure.

CTA-ID : 2003805
Was this helpful?
What can we do to improve the information ?