Technical FAQs

Ask a Question

Will a QO330M125 load center accept a QOT tandem or QO tandem circuit breaker?

No, it will not. QO 3 phase load centers do not accept tandem circuit breakers. This is a 30 space/30 circuit panel, accepting full size QO branch breakers only.

CTA-ID : 2003548
Was this helpful?
What can we do to improve the information ?