Technical FAQs

Ask a Question

Will a QO130M150K load center accept a QOT tandem or QO tandem circuit breaker?<br />

No, it will not. This is a 30 space/30 circuit panel, accepting full size QO branch breakers only.


CTA-ID : 2003541
Was this helpful?
What can we do to improve the information ?