Technical FAQs

Ask a Question

Are alternate lugs available for an EZM1600FS Series M01 Main fusible switch?

Issue:
Product Design Features

Product Line:
EZM Metering Equipment

Environment:
Alternate Main Lugs

Cause:
Application

Resolution:
Yes, This device uses a MHP260006M Molded Case Switch as the Main with Class T fuses.
The standard mechanic lugs that come on the molded case switch from the factory, will accommodate (3) 3/0 - 500kcmil Max. Al/Cu wires per phase and neutral.

Mechanical Lugs:
1) For (2) 600kcmil Al/Cu Max. per phase and neutral use lug kit AL800MA7 for the Molded Case Switch(requires 2 lugs) and lug kit MMLK250 for the main neutral(requires One kit).
2) For (2) 750kcmil Al/Cu Max. per phase and neutral use lug kit AL800MA7 for the Molded Case Switch(requires 2 lugs) and lug landing kit MMSK2 with the ILSCO lug TA8002N(Purchased separate).
3) For (4) 350kcmil Al/Cu Max. per phase and neutral use lug kit AL1000MA for the Molded Case Switch(requires 2 lugs) and the standard neutral Lugs that come on the device.


NOTE: THE MAIN NEUTRAL OF THIS DEVICE WILL NOT ACCEPT COMPRESSION LUGS, SO NO ALTERNATE COMPRESSION LUGS ARE AVAILABLE.

 
Was this helpful?
What can we do to improve the information ?