Technical FAQs

Ask a Question

What is part number for a protective boot which is taller than a 9001KU1 thru 8 boot?<br />

9001KU1 to 8 is .69`` tall compared to 9001KU37 which is 1.36`` tall or a 9001KU47 which is 1.61`` tall. The boots are designed for use with specific operator types.

CTA-ID : 2004031
Was this helpful?
What can we do to improve the information ?