Technical FAQs

Ask a Question

What is the L5 suffix?*

The device with the L5 suffix will have a 5m cable instead of the standard 2m. The suffix is sometimes shown as L05.


CTA-ID : 2003768
Was this helpful?
What can we do to improve the information ?