Technical FAQs

Ask a Question

What is the boot material used in a XACA9412?

It is a watertight, corrosion resistant, polychloroprene and is resistant to ultraviolet light.


CTA-ID : 2004293
Was this helpful?
What can we do to improve the information ?