Technical FAQs

Ask a Question

What is the audible sound level (dB) of the XVAC921 and can it be adjusted? NOTE: This product is obsolete.

Issue:
What is the audible sound level  (dB) of the XVAC921 and can it be adjusted?

Product Line:
Harmony Signalling

Environment:
All products

Cause:
Product Features

Resolution:
It is 90 dB and not adjustable. NOTE:  This product is obsolete.


CTA-ID : 2004022
Was this helpful?
What can we do to improve the information ?