Technical FAQs

Ask a Question

What is the terminal lug data for a QMB327WT3?

Issue:
What is the terminal lug data for a QMB327WT3?

Product Line:
QMB Panelboard, switchboard with QMB distribution.

Environment:
Products sold in the United States.

Cause:
Product features.

Resolution:
The lugs on this device will accept (3) #3/0 AWG - 600 kcmil aluminum or copper conductors per phase.


CTA-ID : 2004013

Was this helpful?
What can we do to improve the information ?