Technical FAQs

Ask a Question

How do you order a XCMA or B with additional cable?

Add the cable length amount in Meters to the end of the part number. XMB502(6)
(6) = 6 meters of cable.

Note standard cable lenght is 1 Meter long.

CTA-ID : 2001918
Was this helpful?
What can we do to improve the information ?