Technical FAQs

Ask a Question

What is the Terminal Lug Data for a SU3040D400K Combination Service Entrance Device?

This device is supplied with line and neutral lug landings for use with compression or mechanical type lugs. For mechanical lugs, use lug kit CMELK4. This lug kit consists of four lugs capable of terminating (1) #2 AWG - 600 kcmil aluminum or copper conductors. Optional mechanical lugs listed on the device wiring diagram include: ILSCO TA-600-2N (#2 AWG - 600 kcmil aluminum or copper) or Anderson L2D2-350 (2 - #6 AWG - 350 kcmil aluminum or copper). Optional crimp lugs: Anderson VHCL-600-12BN (250 - 600 kcmil copper).

CTA-ID : 2003751
Was this helpful?
What can we do to improve the information ?