Technical FAQs

Ask a Question

Is there anything that describes all products by their Class and Type numbers?

Yes, there is a document called the Master Class list. It is posted on the web and contains all Class numbers, if they were used, obsolete, or available, and a brief description of the device. It does not reference the Type numbers.

This does not provide information on devices sold without Class numbers. Nor does this document necessarily indicate who currently supports a given product.

CTA-ID : 2003515
Was this helpful?
What can we do to improve the information ?