Technical FAQs

Ask a Question

Does Square D offer a 3 position horizontal ganged meter socket?<br /><br /><br />

Square D does offer 3 position horizontal gang units, as well as other 2 through 6 position horizontal gang units, not listed in the current Digest. These horizontal gang units are utility company specific catalog numbers and should be verified as approved by the utility company before ordering. Contact the Lexington Product Support Group for inquiries on catalog numbers that do not appear in the current Digest.


CTA-ID : 2004283
Was this helpful?
What can we do to improve the information ?