Technical FAQs

Ask a Question

Where is the date code on the KA I-Line breaker, to tell how old it is?

Issue:
Where is the date code on the KA I-Line breaker, to tell how old it is.

Product Line:
Circuit Breakers.

Environment:
Products sold in the United States.

Cause:
Product features.

Resolution:
It depends on the age of the breaker. Current production has it on the UL label. On older breakers it may be on the faceplate label, or on older ones yet, on the side.


CTA-ID : 2004001

Was this helpful?
What can we do to improve the information ?