Technical FAQs

Ask a Question

What enclosures are available for an LXIL circuit breaker?

Only one enclosure, LX600AWK, is available for the LXIL frame circuit breaker. Use this enclosure for NEMA 1, NEMA 3R, NEMA 5 or NEMA 12 applications. This enclosure is also applicable to the LXL, LCL, LEL and LIL frame circuit breakers through 600 ampere.

CTA-ID : 2003738
Was this helpful?
What can we do to improve the information ?