Technical FAQs

Ask a Question

What can be used in the place of the 8440 PS power supplies?

We have no power supplies this small at this time. The ABL7`s can be used as a replacement. The ABL7RP1205 has a 5A 12 volt DC output capacity. The 8440 PS12 had a 0.63A 12 volt DC output capacity. A ABL7RP2403 has a 3 amp 24 volt DC output capacity and the 8440PS24 had a .32 A 24 volt DC output.

CTA-ID : 2003987
Was this helpful?
What can we do to improve the information ?