Technical FAQs

Ask a Question

How do you mount class 9012, Nema 4, 4X and 13 pressure switches without a mounting foot option?

Customer will need to remove front cover and mount using mounting holes cast into the base.


CTA-ID : 2003724
Was this helpful?
What can we do to improve the information ?