Technical FAQs

Ask a Question

Is the D326N or D326NR safety switch suitable for use as service equipment?

Issue:
Application

Product Line:
General Duty Safety Switch

Cause:
Application

Resolution:
Yes, this switch is marked ``suitable for use as service equipment``. For service equipment use, the neutral should be bonded to the enclosure with the bonding strap provided.


CTA-ID : 2003719
Was this helpful?
What can we do to improve the information ?