Technical FAQs

Ask a Question

Are the standard lugs provided on General Duty, Heavy Duty and Double throw safety switches mechanical or compression type?

Issue:
Product Design Features

Product Line:
General Duty, Heavy Duty and Double Throw Safety Switches

Environment:
Main Lugs

Cause:
understanding

Resolution:
The Standard lugs supplied with ALL Safety Switches will be mechanical Set-Screw type lugs. Compression lugs MAY only be available as an option, depending on the switch catalog number.

NOTE: Most Distribution Equipment will come standard with mechanical set-screw type lugs. 

 
Was this helpful?
What can we do to improve the information ?