Technical FAQs

Ask a Question

What is the contact state for the 9034LLH float switch?

9034LLH has normally closed contacts in the horizontal position.
Depending on how the switch is mounted on the tank will determine if the finger will go up or down. With a 30 degree bend up or down will open the contacts.

CTA-ID : 2003497
Was this helpful?
What can we do to improve the information ?