Technical FAQs

Ask a Question

Can a switch rated at 415 volts be used at 480 volts?<br />

No. The applied voltage can never be greater than the device rating.


CTA-ID : 2003496
Was this helpful?
What can we do to improve the information ?