Technical FAQs

Ask a Question

What is the maximum amperage of equipment that the SDSA1175 Secondary Surge Arrestor can be applied?

The SDSA1175 is not restricted by the ampacity of the equipment or service. being protected.


CTA-ID : 2003965
Was this helpful?
What can we do to improve the information ?