Technical FAQs

Ask a Question

What is form N5 on a 9038JG6N5?

Form N5 is the addition of a third warning signal switch (single pole). Class 9038AG, AR, AW, CG & DG only. It is not available on JG alternators.


CTA-ID : 2003709
Was this helpful?
What can we do to improve the information ?