Technical FAQs

Ask a Question

What enclosures are available for an LCL circuit breaker?

Only one enclosure, LX600AWK, is available for the LCL frame circuit breaker. Use this enclosure for NEMA 1, NEMA 3R, NEMA 5 or NEMA 12 applications. This enclosure is also applicable to the LXL, LXIL, LEL and LIL frame circuit breakers through 600 ampere.


CTA-ID : 2003693
Was this helpful?
What can we do to improve the information ?