Technical FAQs

Ask a Question

Is a NEMA 3R Homeline Load Center Value Pack available?

Yes, HOMVPRB1 consists of a HOM2040M200RB load center, (6) HOM115, (6) HOM120, (1) HOM230 and (1) HOM250 branch circuit breakers


CTA-ID : 2003692
Was this helpful?
What can we do to improve the information ?