Technical FAQs

Ask a Question

What types of connector are used on CM breakers?

Compact CM breakers are bus-connected only. Rear connectors are included when required (2000-2500A UL; 3200A IEC), and are available for purchase as replacements or for rear connection of lower-amperage breakers if desired.
For cable connection, lugs can be applied to customer-supplied bus using customer-supplied mechanical lugs or compression connectors.

CTA-ID : 2003489
Was this helpful?
What can we do to improve the information ?