Technical FAQs

Ask a Question

Can the Square D 690UVTD be used with a Compact NSF breaker and a 29386 MN (120Vac UVR)?

Yes. The 690UVTD is UL listed and will work with the NSF 120Vac UVR (MN). The time delay is likely to be half-again as long as indicated on the unit because of the difference in current draw between the 1121 UVR and the 29386. It works only on 120Vac systems.

CTA-ID : 2003488
Was this helpful?
What can we do to improve the information ?