Technical FAQs

Ask a Question

Does a UT5R1131B include lugs?

Yes, the main lugs and branch lugs are included. The main lugs will accept (1) #6 AWG - 350 kcmil, aluminum or copper conductors, per phase and neutral. The branch lugs will accept (1) #8 - 2/0 AWG, aluminum or copper conductors, per phase and neutral.


CTA-ID : 2003478
Was this helpful?
What can we do to improve the information ?