Technical FAQs

Ask a Question

Does a UT2R2122B include lugs?

Issue:
Product Technical Data

Product Line:
Meter Sockets

Cause:
Lug data required

Resolution:
Yes, the supply side lugs and load side lugs for both tenants are included. The supply side lugs will accept (1) #6 AWG - 250 kcmil, aluminum or copper conductors, per phase and neutral. The load side lugs will accept (1) #8 AWG - 250 kcmil, aluminum or copper conductors, per phase and neutral.


CTA-ID : 2003475
Was this helpful?
What can we do to improve the information ?