Technical FAQs

Ask a Question

Are PG breakers 100% rated or 80% rated.

Can be both depending on the part number selected.


CTA-ID : 2004228
Was this helpful?
What can we do to improve the information ?